AXIS#.MOTOR.NAME

Description

This parameter is the motor name.

 

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

20 chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.NAME

6237

185D

String

Read Only

-

AXIS2.MOTOR.NAME

71773

1185

String

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.NAME

6237

String

Read Only

-